PD2-C-IP CANopen Online Manual

Technical Manual PD2C-IP

Fieldbus: CANopen

For use with the following variants:
  • PD2-C411L18-E-65-08
  • PD2-CB42CD-E-65-08

Valid for firmware version FIR-v1650 and higher Manual version 2.0.0
and hardware version W002 and higher  

Introduction

The PD2-C-IP is a brushless motor with integrated controller in protection class IP65. The integrated absolute encoder makes immediate operation possible in closed loop mode without homing.

This manual describes the functions of the controller and the available operating modes. It also shows how you can address and program the controller via the communication interface.

You can find further information on the device on the Nanotec website us.nanotec.com.

Version information


Manual version Date Changes Firmware version Hardware version
1.0.0 01/2018 First edition FIR-v1650 W002

Copyright, marking and contact

Copyright © 2013 – 2018 Nanotec® Electronic GmbH & Co. KG. All rights reserved.

Nanotec® Electronic GmbH & Co. KG

Kapellenstraße 6

D-85622 Feldkirchen/Munich

 

Phone: +49 (0)89-900 686-0

Fax: +49 (0)89-900 686-50

 

Internet: us.nanotec.com

 

Intended use

The PD2-C-IP motor with integrated controller is designed for use under the approved Environmental conditions.

Any other use is considered unintended use.

Note: Changes or modifications to the product are not permitted.

Warranty and disclaimer

Nanotec produces component parts that are used in a wide range of industrial applications. The selection and use of Nanotec products is the responsibility of the system engineer and end user. Nanotec accepts no responsibility for the integration of the products in the end system.

Under no circumstances may a Nanotec product be integrated as a safety controller in a product or construction. All products containing a component part manufactured by Nanotec must, upon delivery to the end user, be provided with corresponding warning notices and instructions for safe use and safe operation. All warning notices provided by Nanotec must be passed on directly to the end user.

Our general terms and conditions apply: en.nanotec.com/service/general-terms-and-conditions/.

Specialist staff

Only specialists may install, program and commission the device:

  • Persons who have appropriate training and experience in work with motors and their control.
  • Persons who are familiar with and understand the content of this technical manual.
  • Persons who know the applicable regulations.

Other applicable regulations

In addition to this technical manual, the following regulations are to be observed:

  • Accident-prevention regulations
  • Local regulations on occupational safety

EU directives for product safety

The following EU directives were observed:

  • RoHS directive (2011/65/EU, 2015/863/EU)
  • EMC directive (2014/30/EU)

Used icons

All notices are in the same format. The degree of the hazard is divided into the following classes.

CAUTION:
  • The CAUTION notice indicates a possibly dangerous situation.
  • Failure to observe the notice may result in moderately severe injuries.
  • Describes how you can avoid the danger.
Note:
  • Indicates an error source or likelihood of confusion.
  • Failure to observe the notice may result in damage to this or other devices.
  • Describes how device damage can be avoided.
Tip: Shows a tip for the application or task.

Emphasis in the text

The following conventions are used in the document:

Text set in bold indicates cross references and hyperlinks:

Text set in italics marks named objects:

  • Read the installation manual.
  • Use the Plug & Drive Studio software to perform the auto setup.
  • For software: You can find the corresponding information in the Operation tab.
  • For hardware: Use the ON/OFF switch to switch the device on.

A text set in Courier marks a code section or programming command:

  • The line with the od_write(0x6040, 0x00, 5 ); command has no effect.
  • The NMT message is structured as follows: 000 | 81 2A

A text in "quotation marks" marks user input:

  • Start the NanoJ program by writing object 2300h, bit 0 = "1".
  • If a holding torque is already needed in this state, the value "1" must be written in 3212h:01h.

Numerical values

Numerical values are generally specified in decimal notation. The use of hexadecimal notation is indicated by a subscript h at the end of the number.

The objects in the object dictionary are written with index and subindex as follows: <Index>:<Subindex>

Both the index as well as the subindex are specified in hexadecimal notation. If no subindex is listed, the subindex is 00h.

Example: Subindex 5 of object 1003h is addressed with 1003h:05h, subindex 00 of object 6040h with 6040h.

Bits

The numbering of individual bits in an object always begins with the LSB (bit number 0). See the following figure, which uses data type UNSIGNED8 as an example.



Counting direction (arrows)

In figures, the counting direction is always in the direction of an arrow. Objects 60C5h and 60C6h depicted as examples in the following figure are both specified as positive.



Inhalt



Einstellungen zum Datenschutz
Wir verwenden essenzielle Cookies, die für den Betrieb unserer Website erforderlich sind. Mit Ihrer Einwilligung verwenden wir zudem optionale Cookies für Statistik und Marketing. Sie können den nicht-essenziellen Cookies per Klick auf die Schaltfläche „Akzeptieren“ zustimmen oder diese ablehnen. Ihre Einstellungen können Sie jederzeit aufrufen und ihre Zustimmung auch nachträglich widerrufen. Nähere Hinweise hierzu erhalten Sie in unserer Datenschutzerklärung.